The Everis® UQD08 & UQDB08 hybrid set is here.

Scale with our 5-day lead times and capacity to deliver millions of units monthly. Get the speed, capacity, and global support your business demands.

Order Now

of

The Everis® UQD08 & UQDB08 hybrid set is here.
Material
Pressure Range
Mounting Options
Termination Size
Valved?
Sterilization
Termination Type
Seal Options
RFID Enabled

10 Tips for Specifying QDs -- And Why Liquid Cooling Connections Are So Critical

September 14, 2023

Overview

It’s well known that poorly designed thermal management systems can result in suboptimal performance or system failure. What isn’t as well understood are the material properties and myriad calculations that all need to be taken into consideration when developing a high-performing liquid cooling system -- or the role that quick disconnects play in supporting reliability, uptime, ease of maintenance and system performance. It’s complicated but it doesn’t need to be confusing.

CPC’s Application Engineering Manager, Andres Abraham provides tips and insights that will help engineers understand which types of quick disconnects (and other components) are suited for liquid cooling systems. And he will describe how fluid selection decisions should impact the specification of subcomponents in connectors and other system parts in the wetted loop.